How can I install the ZED X on NVIDIA Jetson Xavier NX, Orin NX and Orin Nano devkit?

In order to use the ZED X and the ZED X Mini with NVIDIA Jetson development kits it is necessary to install an additional GMSL2 capture card to provide the required GMSL2 connectivity.

In order to correctly connect the capture card to Xavier/Orin NX and Orin Nano carrier boards you need flat ribbon cables and an external power source, which are not required for the Xavier/Orin AGX models.

To assist you further, we have provided the following guides for your platform:

Attachments: