Can I use the ZED camera on Android?

While we do not officially support using the ZED on Android platforms, the ZEDcamera is a UVC-compliant camera so it is possible to connect the camera to Android phones and tablets with a micro-USB adapter.

Please note that most phones and tablets have USB 2.0 ports and the ZED will work in USB 2.0 compatibility mode on these platforms.

Note: The ZED SDK is not available on Android.