How do I record from the ZED SDK/ZEDfu for offline processing?

The ZED SDK and ZEDfu accepts two types of inputs: live images from the ZED camera or recorded video files from the ZED camera (called Offline Processing).

Record video files with the ZED

Open the ZED Explorer tool and hit the record button to start recording video files. The video sequence is saved with our proprietary SVO format.

SVO files contain all the required information to simulate a live camera within the ZED SDK. 

Should I use offline processing?

The advantages of the Offline Processing method are the following ones:

  • No NVIDIA GPU is required. The recording computer only needs a USB 3.0 port and an i5 or higher CPU. Most of our users use an INTEL NUC or a Jetson TX2.
  • This method offers the possibility to tune the SDK parameters in order to generate different outputs from the same video sequence.
  • Finally, it is the most lightweight setup.

The disadvantages are the following ones:

  • While recording, you have a live view of the camera images, however, no preview of what the 3D scan or the depth will look like.
  • With an NVIDIA-enable recording PC, H.264 or H.265 compressions can be used to lower the SVO ile size, however, without NVIDIA capabilities, the SVO file size will be larger due to less-efficient compression.

 

For example, we recommend the offline setup for scanning applications.
As a reminder, the ZED can be used on Windows 7-10 and Ubuntu 16-18. (not OSX)