What are the credentials to login into the Edge AI Gateway?

The Edge AI Gateway is powered by an Nvidia Jetson TX2 NX or an Nvidia Jetson Xavier NX module running a Ubuntu-derived OS customized by Nvidia to exploit the potentiality of the Jetson devices.

When you boot the system, the default configuration requires you to log in by using the default credentials:

  • Username: user
  • Password: admin

You can change the default credentials after the login by entering the "Settings" menu and selecting the "Users" voice.