How can I install the ZED X cameras on NVIDIA® Jetson™ development kits?
To use the GMSL2 cameras (ZED X, ZED X Mini, ZED X Nano, ZED X One GS, ZED X One S, and ZED X One 4K) with an NVIDIA® Jetson™ development kit, you must install a ZED Link GMSL2 capture card, which provides the GMSL2 connectivity, and the ZED X Driver. GMSL2 cameras are not compatible with USB.
To connect the capture card to the Jetson™ carrier board, you may need flat ribbon cables and an external power source, depending on the card and the development kit.
Choose the capture card
Capture card | Cameras | Compatible development kits |
|---|---|---|
1 | Jetson Orin Nano / Orin NX | |
up to 4 | Jetson Orin Nano / Orin NX, Jetson AGX Orin | |
up to 8 | Jetson AGX Orin |
Setup steps
Install the ZED Link capture card on the Jetson development kit and install the ZED X Driver, following the setup guide of your capture card and development kit (see the list below).
Install the ZED SDK for your JetPack / Jetson Linux version from the ZED SDK download page. To check your version, see What is the version of the OS running on my ZED Box or NVIDIA Jetson embedded PC?
Get started with your camera with its documentation: ZED X family or ZED X One.
Setup guides
If you encounter any issue during the setup, contact us at support@stereolabs.com.
Other options
Ready-to-use embedded PC: the ZED Box series integrates the GMSL2 connectivity, the drivers, and the ZED SDK, with no additional capture card or cabling. The ZED Box 2 and the ZED Box 2 Max (T4000 / T5000) support up to 8 GMSL2 cameras.
NVIDIA® Jetson AGX Thor™ Developer Kit: the Developer Kit does not support the ZED Link GMSL2 capture cards; see Can I use GMSL2 cameras with the NVIDIA Jetson AGX Thor Developer Kit?
ZED X One Core (MIPI): the ZED X One Core connects through the ZED Link MIPI Quad capture card; see the ZED Link MIPI documentation.
Third-party carrier boards: carrier boards with GMSL2 deserializers are available from our partners.