What is the IP rating of the ZED 2i and ZED X and what does it mean?

Several ZED cameras have an IP (Ingress Protection) rating, certifying their resistance to dust and water:

Camera

IP rating

Meaning

ZED 2i

IP66

Dust-tight; protected against powerful water jets (e.g. heavy rain, thunderstorms)

ZED X, ZED X Mini

IP67

Dust-tight; protected against temporary immersion up to 1 m for 30 minutes

ZED X One S (Fisheye, Wide, and Narrow lenses)

IP69K

Dust-tight; protected against close-range, high-pressure, high-temperature water jets (e.g. wash-down cleaning)

Note: since Q4 2026, the ZED X One S is IP69K rated with all the lens options (Fisheye, Wide, and Narrow). The ZED X One S version without lens has no IP rating, because the protection depends on the lens assembly.

For the IP rating of the other models, please refer to the datasheet available on each product page of the StereoLabs store.

What is an IP rating?

IP ratings are defined by the international standard IEC 60529 (Degrees of protection provided by enclosures, IP Code), also published as EN 60529. The first digit indicates the protection against solid particles (6 = dust-tight, the highest level); the second digit indicates the protection against water:

  • 6: powerful water jets (12.5 mm nozzle, 100 l/min) from any direction;

  • 7: temporary immersion, up to 1 m depth for 30 minutes;

  • 8: continuous immersion beyond 1 m, under conditions specified by the manufacturer;

  • 9K: close-range, high-pressure (8 to 10 MPa), high-temperature (80 °C) water jets.

How can I further protect my camera?

  • IP67 protects against temporary immersion only; ZED cameras are not designed for continuous underwater operation. For underwater use, see Can I use the ZED camera underwater?

  • If you plan to use your camera outdoors 24/7, we suggest installing a top cover that limits the amount of direct water hitting the case for prolonged periods.

  • The IP rating is guaranteed only with the cable correctly connected and its connector fully tightened.