What are the advantages of StereoLabs ZED stereo cameras over other depth cameras (e.g., Intel RealSense)?

ZED cameras are passive depth sensors based on stereo vision: depth is computed from two synchronized images, like human binocular vision. Unlike active sensors, they do not emit any laser, IR pattern, or Time-of-Flight signal. This design brings several concrete advantages.

No interference, indoors and outdoors

ZED cameras do not project any light, so multiple cameras can work in the same area at the same time without cross-interference, a key requirement for multi-camera and multi-robot setups. For the same reason, they are not affected by sunlight and work reliably outdoors, where IR-based active sensors typically fail or have a drastically reduced range.

Long depth range

Active sensors are limited to short ranges for physical reasons (emitter power, eye safety, IR reflectivity). The range of a stereo camera scales with resolution, focal length, and baseline, so ZED cameras measure depth at much longer distances, and you can choose the model that fits your working range:

  • ZED 2i and ZED X: long-range perception for outdoor robots and vehicles, with a narrow 4.6 mm lens option to further extend the range;

  • ZED X Mini: short baseline for close-range manipulation and precision tasks;

  • ZED X Nano: compact and lightweight, designed for robotic arms (visual servoing, object picking, end-effector monitoring) with high short-range accuracy;

  • ZED X One GS, ZED X One S, and ZED X One 4K: monocular GMSL2 cameras that can be paired in a custom stereo rig, with a user-defined baseline to extend the depth range even further; see Setting up your stereo rig with two ZED X One cameras.

For the depth range and accuracy of each model, see What is the depth range of the ZED cameras?

AI-powered depth: the Neural Depth Engine

The ZED SDK includes the Neural Depth Engine, an AI-based stereo matching technology that produces dense, accurate, and temporally stable depth maps, even on low-texture surfaces (white walls, floors, uniform objects) that are historically challenging for stereo vision. Depth quality keeps improving with each SDK release through software updates, with no hardware change required.

Perfect image and depth alignment

Depth is computed directly from the images, so the left image and the depth map are natively aligned: the same pixel coordinates address the same physical point in both. There is no need for extrinsic registration between an RGB sensor and a separate depth sensor, and no risk of misalignment over time.

High resolution and frame rate

ZED cameras provide high-resolution depth compared to active sensors: up to 2K on the USB 3 models, and 1920x1200 at 60 FPS with global shutter sensors on the ZED X family, for sharp, distortion-free images even on fast-moving platforms.

A complete software ecosystem

The ZED SDK provides much more than depth, all natively aligned to the same camera reference frame:

Industrial-grade hardware options

Beyond the USB 3 cameras, the ZED X family offers a GMSL2 interface for low-latency, reliable transmission over long cables (up to 15 m), hardware synchronization of multiple cameras, IP67-rated enclosures (ZED X and ZED X Mini), and built-in IMUs. Together with NVIDIA® Jetson™ platforms and the ZED Box embedded PCs, they are suitable for 24/7 deployment on industrial robots and vehicles.