Setting up your Stereo Rig with two ZED X One cameras

The monocular cameras of the ZED X One family (ZED X One GS, ZED X One S, ZED X One 4K, and ZED X One Core) allow the creation of configurable stereo rigs with custom baselines, the distance between the optical centers of the two cameras.

Dual Camera Mount for ZED X One

Lens options

Lens

Focal length

Aperture

Field of view (H x V x D)

Available on

Wide

2.2 mm

f/2.2

110° x 80° x 120°

ZED X One GS, ZED X One S, ZED X One Core

Narrow

4.6 mm

f/2.0

73° x 45° x 87°

ZED X One GS, ZED X One S, ZED X One Core

Fisheye

1.38 mm

f/2.0

204° x 137° x 218°

ZED X One S, ZED X One Core

Wide (4K)

3.1 mm

f/2.0

110° x 72° x 119°

ZED X One 4K

The wide, narrow, and 4K lenses follow a pinhole (rectilinear) projection model. The fisheye lens follows a fisheye projection model (f-theta), with a field of view wider than 180°: to compute depth, the fisheye images are rectified to pinhole images with a smaller field of view. For more details, see What is the camera focal length and field of view?

How to calculate the baseline

The value of the baseline depends on the final requirements and on the optics of the two cameras.

In the following scheme, the baseline is identified by B, the minimum depth range is h, and α is the field of view of the cameras for the rectified images.

Stereo rig field of view, baseline, and minimum depth

For a fixed minimum depth value h, you can calculate the required baseline B as:

B = 2 * h * tan(α/2)

Vice versa, if you fix the baseline B, the corresponding minimum depth value h is:

h = B / (2 * tan(α/2))

To obtain a minimum depth that allows a usable depth map, apply a factor of 6 to h. This guarantees that the fields of view of the two cameras have a large enough overlapping area:

h' = 6 * h ; B' = B / 6

The maximum depth (in meters) can be calculated with the formula:

max_depth = (B / 2) * (F / sens_w) * res_W

where:

  • B is the baseline in meters;

  • F is the focal length of the lens in meters (2.2 mm for the wide lens and 4.6 mm for the narrow lens of the ZED X One GS, ZED X One S, and ZED X One Core; 3.1 mm for the ZED X One 4K);

  • sens_w is the width of the CMOS sensor in meters (5.8 mm for the global shutter sensor, 7.7 mm for the 4K sensor);

  • res_W is the image width in pixels (you can use 1280 as a good approximation).

For the fisheye lens, use α and the equivalent focal length of the rectified images instead of the nominal values: with a rectified horizontal field of view of 120°, α = 120° and F / sens_w = 1 / (2 * tan(60°)) ≈ 0.29.

How to choose the right sensor?

The global shutter sensor (ZED X One GS, ZED X One S, ZED X One Core) is best for fast-moving objects, or a fast-moving camera, and for applications that require accurate motion reproduction.

The rolling shutter 4K sensor (ZED X One 4K) is best for low-light environments and for high-resolution HDR images.

How to choose the lens?

The field of view of the lenses has a direct impact on the system performance, so choose it according to the requirements of your application:

  • Narrow lenses provide greater detail and are well suited for long-range detection.

  • Wide lenses are best for applications requiring broader coverage.

  • Fisheye lenses (ZED X One S and ZED X One Core) provide maximum field awareness, with a field of view of more than 180°, for short-range perception and wide-area monitoring. The large field of view comes with strong image distortion and lower angular resolution, which reduce the detail and the depth accuracy at long range compared to the wide and narrow lenses.

Narrow and wide FOV comparison

How to choose the baseline?

The baseline of the stereo system depends on the required depth perception. A larger baseline improves the depth resolution, but increases the minimum distance for accurate depth estimation. The following tables provide an estimate of the depth accuracy at different distances, depending on the baseline and the lens option.

How to read the tables:

  • plain values are in the recommended zone (depth error below 5% of the distance);

  • italic values are available, but the depth error is 5% or more of the distance;

  • "–" means that depth is not available for that combination of baseline and distance.

ZED X One GS, ZED X One S, and ZED X One Core with wide lens (2.2 mm)

Baseline \ Distance

10cm

30cm

50cm

75cm

1m

1.5m

2m

3m

4m

5m

7m

10m

20m

25m

50m

100m

200m

300m

3cm

<1mm

1mm

4mm

8mm

15mm

34mm

6cm

14cm

24cm

38cm

74cm

–

–

–

–

–

–

–

7cm

–

1mm

2mm

4mm

6mm

14mm

3cm

6cm

10cm

16cm

32cm

64cm

–

–

–

–

–

–

15cm

–

–

1mm

2mm

3mm

7mm

1cm

3cm

5cm

8cm

15cm

30cm

1.20m

1.88m

–

–

–

–

25cm

–

–

–

1mm

2mm

4mm

1cm

2cm

3cm

5cm

9cm

18cm

72cm

1.13m

4.51m

–

–

–

50cm

–

–

–

–

–

2mm

<1cm

1cm

1cm

2cm

4cm

9cm

36cm

56cm

2.25m

9.02m

–

–

75cm

–

–

–

–

–

–

<1cm

1cm

1cm

2cm

3cm

6cm

24cm

38cm

1.50m

6.01m

–

–

1m

–

–

–

–

–

–

–

<1cm

1cm

1cm

2cm

5cm

18cm

28cm

1.13m

4.50m

18.04m

–

1.5m

–

–

–

–

–

–

–

–

<1cm

1cm

1cm

3cm

12cm

19cm

75cm

3.00m

12.01m

27.05m

2m

–

–

–

–

–

–

–

–

–

1cm

1cm

2cm

9cm

14cm

56cm

2.25m

9.00m

20.27m

ZED X One GS, ZED X One S, and ZED X One Core with narrow lens (4.6 mm)

Baseline \ Distance

10cm

30cm

50cm

75cm

1m

1.5m

2m

3m

4m

5m

7m

10m

20m

25m

50m

100m

200m

300m

3cm

–

1mm

2mm

5mm

9mm

20mm

3cm

8cm

14cm

22cm

43cm

87cm

–

–

–

–

–

–

7cm

–

<1mm

1mm

2mm

4mm

8mm

1cm

3cm

6cm

9cm

18cm

37cm

1.49m

2.33m

–

–

–

–

15cm

–

–

–

1mm

2mm

4mm

1cm

2cm

3cm

4cm

9cm

17cm

69cm

1.09m

4.35m

–

–

–

25cm

–

–

–

–

1mm

2mm

<1cm

1cm

2cm

3cm

5cm

10cm

42cm

65cm

2.61m

10.45m

–

–

50cm

–

–

–

–

–

–

<1cm

<1cm

1cm

1cm

3cm

5cm

21cm

33cm

1.30m

5.21m

20.90m

–

75cm

–

–

–

–

–

–

–

<1cm

1cm

1cm

2cm

3cm

14cm

22cm

87cm

3.47m

13.91m

31.35m

1m

–

–

–

–

–

–

–

–

<1cm

1cm

1cm

3cm

10cm

16cm

65cm

2.61m

10.43m

23.48m

1.5m

–

–

–

–

–

–

–

–

–

–

1cm

2cm

7cm

11cm

43cm

1.74m

6.95m

15.64m

2m

–

–

–

–

–

–

–

–

–

–

–

1cm

5cm

8cm

33cm

1.30m

5.21m

11.73m

ZED X One S and ZED X One Core with fisheye lens (1.38 mm), rectified to a 120° horizontal field of view

Baseline \ Distance

10cm

30cm

50cm

75cm

1m

1.5m

2m

3m

4m

5m

7m

10m

20m

25m

50m

100m

200m

300m

3cm

<1mm

2mm

5mm

11mm

20mm

45mm

8cm

18cm

32cm

50cm

–

–

–

–

–

–

–

–

7cm

–

1mm

2mm

5mm

9mm

19mm

3cm

8cm

14cm

21cm

42cm

86cm

–

–

–

–

–

–

15cm

–

<1mm

1mm

2mm

4mm

9mm

2cm

4cm

6cm

10cm

20cm

40cm

1.60m

2.50m

–

–

–

–

25cm

–

–

1mm

1mm

2mm

5mm

1cm

2cm

4cm

6cm

12cm

24cm

96cm

1.50m

–

–

–

–

50cm

–

–

–

–

1mm

3mm

<1cm

1cm

2cm

3cm

6cm

12cm

48cm

75cm

3.00m

–

–

–

75cm

–

–

–

–

–

2mm

<1cm

1cm

1cm

2cm

4cm

8cm

32cm

50cm

2.00m

7.99m

–

–

1m

–

–

–

–

–

–

<1cm

1cm

1cm

1cm

3cm

6cm

24cm

37cm

1.50m

5.99m

–

–

1.5m

–

–

–

–

–

–

–

<1cm

1cm

1cm

2cm

4cm

16cm

25cm

1.00m

3.99m

15.97m

–

2m

–

–

–

–

–

–

–

–

<1cm

1cm

1cm

3cm

12cm

19cm

75cm

3.00m

11.98m

26.96m

The fisheye values are a theoretical estimate for images rectified to a 120° horizontal field of view; a wider rectified field of view reduces the minimum depth, but also the depth accuracy and the maximum range.

ZED X One 4K with wide lens (3.1 mm)

Baseline \ Distance

10cm

30cm

50cm

75cm

1m

1.5m

2m

3m

4m

5m

7m

10m

20m

25m

50m

100m

200m

300m

3cm

<1mm

1mm

4mm

8mm

14mm

32mm

6cm

13cm

23cm

36cm

70cm

–

–

–

–

–

–

–

7cm

–

1mm

2mm

3mm

6mm

14mm

2cm

5cm

10cm

15cm

30cm

61cm

–

–

–

–

–

–

15cm

–

–

1mm

2mm

3mm

6mm

1cm

3cm

5cm

7cm

14cm

28cm

1.14m

1.78m

–

–

–

–

25cm

–

–

–

1mm

2mm

4mm

1cm

2cm

3cm

4cm

8cm

17cm

68cm

1.07m

4.28m

–

–

–

50cm

–

–

–

–

–

2mm

<1cm

1cm

1cm

2cm

4cm

9cm

34cm

53cm

2.14m

8.55m

–

–

75cm

–

–

–

–

–

–

<1cm

1cm

1cm

1cm

3cm

6cm

23cm

36cm

1.42m

5.70m

22.84m

–

1m

–

–

–

–

–

–

–

<1cm

1cm

1cm

2cm

4cm

17cm

27cm

1.07m

4.27m

17.11m

38.58m

1.5m

–

–

–

–

–

–

–

–

<1cm

1cm

1cm

3cm

11cm

18cm

71cm

2.85m

11.39m

25.66m

2m

–

–

–

–

–

–

–

–

–

1cm

1cm

2cm

9cm

13cm

53cm

2.13m

8.54m

19.23m

Accessories

In the StereoLabs store, you can find the Dual Camera Mount for ZED X One, an aluminum bar to create precise stereo rigs with two ZED X One GS or ZED X One 4K cameras, with a customizable baseline from 52 mm to 222 mm. For the ZED X One S, see the Camera Mount for ZED X One S.

Dual Camera Mount for ZED X One, top viewDual Camera Mount for ZED X One

Calibration

A custom stereo rig must be calibrated before it can be used with the ZED SDK. See the Dual Camera Stereo Vision documentation for the ZED X One GS, S, and 4K, and the ZED X One Core Dual Camera Stereo Vision documentation for the ZED X One Core.