Are there any video/image samples from the ZED products that I can see and test before the purchase?

The ZED SDK allows you to record large video datasets using H.264, H.265, or lossless compression. The SDK uses Stereolabs SVO format to store videos along with additional metadata such as timestamps and sensor data.

When loading SVO files, the ZED API will behave as if a ZED was connected and a live feed was available. Every module of the ZED API will be available: depth, tracking, spatial mapping, and more.

More information about how to use an SVO file with the ZED SDK is available on the online documentation.

Demo SVO files

Example meshes generated with Spatial Mapping

If you have any difficulties, mail us your questions at support@stereolabs.com