Documentazione
Affronta le sfide senza sforzo con la nostra sezione documentazione. Accedi a soluzioni di esperti e consigli pratici per una risoluzione dei problemi senza intoppi.
Articles
- Do the ZED cameras support capturing and saving raw data of RGB sensor ? (e.g. bayer pattern dataset without nonlinear processing)?
- Is it possible to genlock the ZED cameras to a cinema camera so that a 100% synchronized depth image is captured for each image capture by the main camera?
- What is the readout time of the ZED 2 camera?
- Where can I find documentation for the ZED?
- Are there any benchmarks on the speed (in FPS or ms/pose) with regards to your pose estimation module for the ZED cameras?
- Are there any video/image samples from the ZED products that I can see and test before the purchase?
- Is the object recognition running on the AI built into the camera, or on the development platform (PC, Embedded Linux devices etc)?