SDK 模块:跟踪、建图、AI 与 GNSS
使用 ZED SDK 进行位置追踪、空间映射、AI 模型优化、目标检测、IMU 和 GNSS 融合。
Articles
- How can I connect an external GPS / GNSS receiver to ZED cameras to geo-tag the video?
- How can I optimize the ZED SDK AI models manually?
- Are there benchmarks on the speed (FPS) of the ZED SDK positional tracking module?
- Is the object recognition running on the AI built into the camera, or on the development platform (PC, Embedded Linux devices etc)?
- Spatial Mapping Best Practices
- How can I remove the IMU drift of my camera?