What type of GMSL2 cable should I use with my ZED X camera?

Last updated: October 23, 2026

Male FAKRA connector on the back of a ZED X cameraFemale FAKRA connector

All StereoLabs GMSL2 cameras (ZED X, ZED X Mini, ZED X Nano, ZED X One GS, ZED X One S, and ZED X One 4K) have a male FAKRA Z connector on the back of the camera. They require a coaxial cable with at least one female FAKRA connector.

GMSL2 FAKRA connectors overview

The connector on the other side of the coaxial cable depends on your configuration:

Maximum cable length

The maximum total length of the GMSL2 connection is 15 meters; longer connections can cause disconnection issues.

Each cable-to-cable coupling can introduce noise and further reduce the maximum total length. To minimize the number of couplings, use the longest cables that fit your setup.

GMSL2 cable configuration example 1GMSL2 cable configuration example 2GMSL2 cable configuration example 3GMSL2 cable types summary

All the GMSL2 cables are available in the accessories section of the StereoLabs store.