• Docs
  • Developers
  • Community
  • Store
ZED Help Center
  • Docs
  • Developers
  • Community
  • Store
  1. Help Center | Stereolabs
  2. ZED SDK
  3. Documentation

Topics

  • Getting Started
  • FAQ
  • Troubleshooting
  • Orders and Shipping

Related articles

  • What is the camera focal length and field of view?
  • Is the object recognition running on the AI built into the camera, or on the development platform (PC, Embedded Linux devices etc)?
  • How do I convert SVO files to AVI, or image/depth sequences?
  • How do I update my ZED camera firmware?
  • How can I convert 3D world coordinates to 2D image coordinates and viceversa?

Do the ZED products have an auto-exposure functionality?

The ZED product sensors have an auto-exposure option and the depth accuracy is about 1% of the measuring distance.

 

Related articles:

For depth sensing, what is the range for the ZED cameras in terms of measuring distances and the accuracy of the detection?

Is the object recognition running on the AI built into the camera, or on the development platform (PC, Embedded Linux devices, etc)?

 

  • Facebook
  • Twitter
  • LinkedIn
  • Home
  • Help Center
  • Documentation
  • Developers
  • Shop
  • @Stereolabs3d