Documentation
- Are there any video/image samples from the ZED products that I can see and test before the purchase?
- Is it possible to genlock the ZED cameras to a cinema camera so that a 100% synchronized depth image is captured for each image capture by the main camera?
- Do the ZED cameras support capturing and saving raw data of RGB sensor ? (e.g. bayer pattern dataset without nonlinear processing)?
- Are there any benchmarks on the speed (in FPS or ms/pose) with regards to your pose estimation module for the ZED cameras?
- What is the readout time of the ZED 2 camera?
- Is the object recognition running on the AI built into the camera, or on the development platform (PC, Embedded Linux devices etc)? See all 7 articles
API Reference
- For the ZED cameras, is it possible to retrieve a pair of images at different resolutions? For example, getting a HD1080 image from one sensor of the camera and VGA from the other?
- What is the file size for videos recorded by the ZED cameras?
- Can very small objects be detected by the ZED Cameras?
- How to connect an external GPS to the ZED cameras for providing the video with GPS tags?
- Do you have an API reference for the ZED SDK?