Are the ZED cameras compatible with Ubuntu 20.04? Can the device's SDK packages work with Ubuntu 20.04?

The ZED cameras and the SDK are perfectly compatible with Ubuntu 20.04. You would be able to use the camera and the SDK without any issues with the OS.

 

Additional Resources:

How does the ZED work?

Can I use the ZED on mobile, Raspberry Pi, or other platforms?

Is it possible to use the ZED cameras with tablets like the Surface Pro, iPad, and mobile devices, to get 3D mapping? 

Can the ZED 2 be powered over Ethernet (POE) or 12v powering options?