• Docs
  • Developers
  • Community
  • Store
ZED Help Center
  • Docs
  • Developers
  • Community
  • Store
  1. Help Center | Stereolabs
  2. Installation and Getting Started

Installation and Getting Started

Explore our comprehensive installation and getting started section to smoothly begin your journey.

Getting Started

  • Why doesn't the ZED SDK detect my ZED X One?
  • Get started with Jetson Orin Nano (NX) devkit and ZED X / ZED X One cameras
  • How can I install the ZED X on NVIDIA® Jetson development kits?
  • What are the default credentials to login into the ZED Box?
  • Is CUDA required in order to use the ZED cameras in Linux?
  • Getting Started with your ZED camera
  • See all 8 articles

General Information

  • Where can I find the datasheet of my device?
  • Why is there a difference in camera parameters between the ZED SDK API and the ZED Explorer tool?
  • What type of GMSL2 cable should I use with my ZED X camera?
  • Where can I find a comparison table for the ZED Stereo Cameras?
  • Setting up your Stereo Rig with two ZED X One cameras
  • What is the version of the OS running on my ZED Box or NVIDIA® Jetson™ embedded PC?
  • See all 35 articles

ZED Compatibility

  • Can I use the ZED X GMSL2 cameras with the NVIDIA® Jetson AGX Thor development kit?
  • Which graphics cards are supported by the ZED SDK?
  • Can I use the ZED without CUDA?
  • Is the ZED backward-compatible with USB 2.0?
  • Home
  • Help Center
  • Documentation
  • Developers
  • Shop
  • @Stereolabs3d