The ZED Box has no Wi-Fi capabilities out of the shelf, but you can use commercial USB Wi-Fi dongles to add this functionality if you need it.
Following is a list of officially supported USB Wi-Fi dongles:
| Model | Nvidia Jetpack | Performances (Download, Upload, Ping) |
| TP-Link 300 Mbps TL-WN823N | Jetpack 4.6 (*) | D: ~7 Mbps - U: ~ 0.6 Mbps - P: 8 ms |
| TP-Link Archer T2U Plus AC600 | Jetpack 4.6 (*) | D: ~224 Mbps - U: ~ 191 Mbps - P: 6 ms |
| TP-Link Archer T2U Nano AC600 | Jetpack 4.6 (*) | D: ~226 Mbps - U: ~ 165 Mbps - P: 8 ms |
| TP-Link TL-WN722N | Jetpack 4.6 (*) | D: ~36 Mbps - U: ~ 45 Mbps - P: 7 ms |
| Linksys WUSB6400M AC 1200 | Jetpack 4.6 (*) | D: ~262 Mbps - U: ~ 305 Mbps - P: 7 ms |
| Linksys WUSB6300 AC1200 | Jetpack 4.6 (**) | - |
(*) tested in the Stereolabs R&D center
(**) recommended by Nvidia
We suggest you connect the Wi-Fi adapter to the USB2 port.