Can the ZED cameras be used with standalone VR headsets like Pico G2 or Oculus Quest ?

You can find the list of headsets supported here.

 

Note:- that the ZED cameras have to be tethered to a computer and can't be use wireless (or directly plugged into the Headset)

 

Additional Resources:

Can I mount my ZED Mini to a Vive Pro headset?

Is it possible for the ZED cameras to integrate with a WMR headset? Are there unity plug-ins available for developing VR/AR applications?

Which VR headsets are compatible with AR passthrough via ZED Mini?