일반 정보
ZED 제품(USB 카메라, GMSL 카메라 등)에 대한 일반 정보를 살펴보고 여정을 순조롭게 시작하세요.
Articles
- How can I convert 3D world coordinates to 2D image coordinates and viceversa?
- Can the ZED 2 be powered over Ethernet (POE) or 12v powering options?
- How can I capture images/video from the ZED camera for offline processing in ZED SDK/ZED tools?
- Is the ZED camera IR sensitive?
- How can I optimize the ZED SDK AI models manually?
- Why is the depth map so dark?
- Can I connect the ZED X and ZED X Mini to a USB3 port?
- What is the version of the OS running on my ZED Box or NVIDIA® Jetson™ embedded PC?
- Setting up your Stereo Rig with two ZED X One cameras
- What are the GPU requirements for running modules like Object detection, spatial tracking, depth estimation etc using the ZED SDK?
- Where can I find the datasheet of my device?
- What are the advantages of using the Stereolabs ZED stereocameras over other depth cameras (eg. Intel Realsense) available in the market?
- For the depth sensing, what is the range for the ZED cameras in terms of measuring distances and the accuracy of the detection?
- Does the polarizer filter of the ZED2i reduce the incoming light?
- How can I get the serial number of my camera?
- Can I use the ZED Box without an HDMI display?
- What is the IP rating of the ZED 2i and ZED X and what does it mean?
- What is the calibration file?
- How can I recover my camera without unplugging it?
- How do I update my ZED camera firmware?
- Does the ZED 2 camera have noticeable trouble identifying human motion and depth imaging during rain, snow, or other particulates passing through its field of view?
- Can I use the ZED camera underwater ?
- Can the ZED stereocameras detect glass doors or glass walls?
- Can the ZED cameras connect directly to a smartphone? Can I develop an Android application to use with it?
- What is the baseline for the ZED 2i camera? Is it better to use the factory given calibration settings or calibrate the sensor manually?
- What is the camera focal length and field of view?
- Where can I find a comparison table for the ZED Stereo Cameras?
- Where can I get 3D models and dimensions of my device?
- Why is there a difference in camera parameters between the ZED SDK API and the ZED Explorer tool?
- What kind of the shutter mode do the ZED cameras use? Is it a rolling shutter or a global shutter?
- Does the ZED work in low-light environments?
- What type of GMSL2 cable should I use with my ZED X camera?
- Can I get a sample or trial unit of Stereolabs' devices?
- What is the latency of the ZED camera?
- How do I use multiple ZED cameras on one computer?